Open Project File Dialog Box Overview

This dialog box displays when the revision of the project you are trying to open is not compatible with an installed version of the
Logix Designer
application. This dialog box provides you with the appropriate information you need to open your project.
Click the
Change Controller
button to change the revision of the project to one that is compatible with the installed version of the
Logix Designer
application, or to change the controller type.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal