Get Dialog Box Overview

Use this dialog box to retrieve a file.
Parameters
Parameter
Description
Comments
Enter a comment up to 255 characters in length. Comments longer than 255 characters are truncated.
Make writable
If selected, AssetCentre removes the read-only restriction on the file once it is downloaded to the location specified in the To field.
If not selected, the downloaded file is read-only.
To
Identifies the location for the checked out file.
Type a new destination or select the ellipses to enter a new destination for the file.
Working Folder Browse button
Open the Browse for Folder dialog box to choose a working folder.
OK
Start the file get process (if initiated process from the Open/Import Project dialog box).
If the directory specified in the To field does not exist, the
Logix Designer
application prompts to create the directory. If directory is created, AssetCentre uses that directory as the working folder and continues with the get operation. If directory is not created, the Get dialog box appears.
Cancel
Close the Get dialog box without completing the get operation.
Help
View help on the Get dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal