(Interactive Access) Explorer
This section allows you to transfer files between local and remote devices. In
Explorer
you can carry out remote file operations, such as download, upload, rename, and delete files. You can click the play symbol
next to an executable file installed in the remote device to start it.You can monitor file transferring processes through a practical two-panes view, showing both the root and the receiving folder paths.
This section is split in two panes: the left panel displays the files the local device
running the , while the right pane shows the files
the remote device.
FactoryTalk®
Remote Access™
ManagerTo access the
File transfer
pane, proceed as follows:- Make sure that theis connected to the remote device.FactoryTalk® Remote Access™Manager
- Access the section.
- Click theInteractive AccessTool button, then selectExplorer.NOTE: See Interactive Access for further information on this Tool.
NOTE:
File Transfer operates with local system privileges. This means that the admin can enable or disable specific
operations for remote users.
FactoryTalk®
Remote Access™
ManagerOnce you have selected the files that you want to transfer, click
Send
or Receive
, as needed.
NOTE:
In case the file transfer is interrupted for any reason, it can be resumed or restarted by clicking
Resume
or Resume all
.To rename a file or folder, right-click it and select
Rename
in the context menu.Provide Feedback