Routing rules
NOTE:
See the
Networking
section in the User manual of your router for further information on this subject.Routing rules consist of a set of criteria determining the path that data packets take from the source to destination across one or more networks. Routing rules are a fundamental aspect of networking, playing a crucial role in determining how data is transmitted between devices on a network.
Once a remote VPN connection is established, the devices connected to LAN 1 become
immediately reachable. Instead, the devices connected to LAN 2 are accessible only upon
routing rule configuration through .
FactoryTalk®
Remote Access™
ManagerConfiguration
To create, modify and cancel static routing rules through , access and select a device on the left pane. Then, select
FactoryTalk®
Remote Access™
ManagerRouting
rules
on the right pane and click on the circled plus
button.The
Create routing rule
window shows up. It includes three
fields:- Subnet IP: The subnet that you wish to reach.
- Subnet mask: The mask of the subnet that you wish to reach.
- Gateway IP: The gateway to which any requests to access a specific subnet are forwarded.
You can associate a number of routing rules to a device.
Routing Rules are visible only if applied to a device to which the user is connected, and
if a VPN connection is established.
Routing rules are visible in the other than in the .
Routing rules
section of the right
pane of the FactoryTalk®
Remote Access™
ManagerIn the example shown, one static routing rules has been applied.
NOTE:
When a VPN connection is no longer active, the added routing rules
are automatically deleted.
Example
To allow the computer that provides remote assistance through to reach endpoints 4, 5 or 6,
configure a routing rule as follows:
FactoryTalk®
Remote Access™
Manager- Subnet IP: 10.65.0.0
- Subnet Mask: 255.255.0.0
- Gateway IP: 192.168.11.113
Provide Feedback