Create a project
A project contains elements with which a
FactoryTalk Optix Application
is
made.- In the main toolbar, selector open
ProjectFactoryTalk Optix Studio.The Start page opens. - SelectNew.
- Select the project type:TIP: The selected project type does not affect any deployment capabilities. You can deploy any project type to any target device type. For more information, see Deploying projects.
- Default. Create a project with all configured categories and a main window inProject view.
- OptixPanel. Create a project with all configured categories and a main window inProject viewand:
- ASystemobject with a pre-configuredFT Remote Accesswidget to request access to the FactoryTalk Remote Access server and assistance from the FactoryTalk Remote Access application.
- ASettingsWidgetsfolder that containsNetwork Settings,Device Settings,Date & Time, andLoad Applicationwidgets.
- A main window that displays and allows you to navigate the default widgets at runtime as well as place your own content on the Home page of the window.
- Automatic language switching for widgets.
- An enabled virtual keyboard
- Optix template. Create a project based on the content contained in the user-defined Optix template.
- Blank. To create a blank project that has no default content, inFactoryTalk Optix Studio Options, selectAdvanced modeand then restartFactoryTalk Optix Studioto selectBlankon the Start page. See Set options.
- InName, enter the name of the project.
- InLocation, enter or browse to the project path.The default location isC:\Users\UserName\Documents\RockwellAutomation\FactoryTalk Optix\Projects
- (optional) To encrypt project passwords, custom objects that have thePasswordDataType, andYAMLfiles that represent the project information model, select the option next toSecrets Encryption Modeand then forNew projects secrets encryption, select either:
- Remote key store. Encrypt project secrets by using a remote key store. You need to be logged in toFactoryTalk Huband be a part of a relevant organization.
- User provided password. Encrypt project secrets with a password.
TIP: For more information about secrets encryption and the default project encryption for new projects, see Project secrets encryption and Set options. - UnderSet main window size, specify the width and height of the main window when you create projects:
- SelectCustom sizeand enter a newWidthandHeightfor a new custom window size. The default custom window size is 400 x 400 pixels.
- Select a pre-configured window size.
- Select anOptixPanelsize if you are creating an OptixPanel project.
- SelectCreate.
The new project opens. If there was an existing project already open, the project opens in
a new instance of
FactoryTalk Optix
.project
optix panel
default
blank
window size
Provide Feedback