Leave an Organization
An administrator or contributor can leave an organization. If you are an owner of the organization that you want to leave you need to transfer the organization ownership to another user. See Transfer Organization Ownership.
- To leave an organization:
- From the FactoryTalk Hub menu, selectOrganizations.
- From the list of organizations, select the organization you want to leave and select
. - In the Leave organization section, selectLeave.
- In the pop-up dialog box that appears, selectLeave.The access to the organization is denied and the organization does not appear in the organizations list on the Organizations page.
Provide Feedback