Applications
The Applications page displays all the applications affiliated with an
organization.
To view the Applications page, from the FactoryTalk menu, select
Applications
.Applications are displayed as tiles. FactoryTalk Hub tiles are arranged by sections that
only appear if you have access to an application that would be in that section. For
example, if you have not made any applications favorites you do not see a favorites
section. There is also information and interactivity associated with each tile.
FactoryTalk Hub Tiles and Badges

Tile Type or Badge | Description | Notes |
|---|---|---|
Tile Sections: | ||
Pending for (Org Name) | Tiles for not provisioned services and for which the logged in user
is an Admin or Owner for the organization and has active unallocated
entitlements for the service. | This section only appears for administrators and owners of the
organization. |
Favorites | Tiles marked by the user as Favorites. | |
For you | Displays the tiles for applications that are already provisioned for
the organization, and the user has access and can open them. | |
By request | Displays the tiles for applications that are provisioned for the
organization but the user does not have access to them and cannot
open them. The user must request access from the administrator. | |
More from Rockwell Automation | Displays the rest of tiles for all other applications available in
FactoryTalk Hub that are not provisioned for the organization or are
available for preview only. | |
Icon on tiles: | ||
Star on tile | A filled star indicates that the user has marked it as a favorite.
Once marked, the tile will also appear in the favorites section of
FactoryTalk Hub. | The star appears empty if the application is not selected as a
Favorite |
Purple icon with number inside | Indicates the number of entitlements the user has available to
allocate for that service. | Only appears to Admins or Owners of the organization. |
Red icon with exclamation point inside |
| The purple icon cannot appear when this icon is displayed. |
Action buttons on tiles: | ||
Add+ | Opens View Entitlements screen. | Appears when the logged in user is an Admin or Owner for the
organization and has active, unallocated entitlements for the
service. |
Request | Appears on the tiles visible in the By request section if the
user does not have access to a specific application. By selecting the
Request button, the user requests
access. | |
Open | Opens the application in a new tab | |
Product info | Opens a a pop-up with the product description | |
Set up | Opens the application to complete provisioning workflow. | The logged in user must be an Admin or Owner of the
organization. |
Provide Feedback