Connection View
Use Connection to define controller-to-device behavior:
- Set the RPI rate. For more information, see Requested Packet Interval.
- Select Unicast or Multicast connection to use on the EtherNet/IP network. For more information, see Unicast or Multicast Connection.
- View the reason of Connection Fault.TIP: If there is a connection fault, Connection Fault area displays the error code with description that helps you to troubleshoot the module. For more information, see Troubleshoot Your Module.
- Inhibit the module. For more information, see Module Inhibiting.
- Configure fault response for connection failure while the controller is in Run Mode.
- Enable or disable the Automatic Diagnostics.ATTENTION: If you do not enable Automatic Diagnostics, the device does not publish diagnostics to FactoryTalk Alarms and Events.
Connection View Example

Recommended Minimum RPI Values for Notch Filters
In the following table, each Notch Filter setting has two recommended minimum module
RPI values that allow the required time to collect samples from each channel. One
setting provides faster sample speed and the other provides slightly better
resolution at slower sample speeds.
Notch Filter (Hz) | Recommended Minimum Module RPI
Value | |||
|---|---|---|---|---|
Application That is Configured With
Only One Channel Enabled | Application With All Channels
Enabled and Using the Same Notch Filter Setting on All
Channels | |||
Faster Sampling Speed (ms) | Better Noise Rejection (ms) | Faster Sampling Speed (ms) | Better Noise Rejection (ms) | |
10 | 106 | 316 | 422 | NA |
20 | 53.1 | 158.1 | 212 | 632 |
50 | 22 | 64 | 86 | 254 |
60 (default) | 18.3 | 53.2 | 72 | 212 |
100 | 11.2 | 32.1 | 44 | 127 |
200 | 5.9 | 16.4 | 22.2 | 65 |
400 | 3.5 | 8.6 | 12 | 33 |
500 | 2.8 | 6.9 | 9.3 | 26.5 |
1000 | 1.7 | 3.8 | 5.2 | 13.5 |
5000 | 1.0 | 1.3 | 2.2 | 3.3 |
10000 | 0.7 | 0.9 | 1.7 | 2.1 |
15625 | 0.8 | 0.8 | 1.7 | 1.7 |
31250 | 0.4 | 0.6 | 1.2 | 1.5 |
Minimum RPI Calculation When Using Different Notch Filter Selections
When input channels on the same module use different Notch Filter selections, you
must consider the sample time for each channel. This helps you to find the
recommended RPI that provides enough time for sampling all channels.
Because all input channels in 5034-IF4 share the same Analog to Digital Converter,
the recommended minimum RPI rate for all enabled channels added together is the
recommended minimum module RPI.
Channel | Notch Filter (Hz) | Recommended Minimum Module RPI for Each Channel (ms) | Recommended Minimum Module RPI (ms) |
|---|---|---|---|
Ch00 | 50 | 22 | 24.1 |
Ch01 | 1000 | 1.7 | |
Ch02 - Disabled | N/A | N/A | |
Ch03 | 31250 | 0.4 |
Channel | Notch Filter (Hz) | Recommended Minimum Module RPI for Each Channel (ms) | Recommended Minimum Module RPI (ms) |
|---|---|---|---|
Ch00 | 50 | 64 | 68.4 |
Ch01 | 1000 | 3.8 | |
Ch02 - Disabled | N/A | N/A | |
Ch03 | 31250 | 0.6 |
Provide Feedback