Import > Component command

Choose this command to import the selected Add-On Instruction, data type,
Equipment Phase
,
Equipment Sequence
, program routine, string types or trend.
This command is not available online, a state in which a device is in direct communication (for example, when
Logix Designer
is monitoring the program file in a controller).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal