Print > Controller Organizer command

The Controller Organizer Listing provides you with a report that lists the basic organization of a project as listed in the Controller. The report is broken up into the following sections:
  • Tasks
  • Motion Groups,
  • Add-On Instructions
  • Data Types
  • Trends
  • I/O Configuration
Components that have descriptions are shown with the descriptions displayed underneath the component. There is no information about tag collections in the report.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal