Import/Paste Configuration dialog box - Programs tab

Use this dialog box to view program definitions during an import.
TIP: To open the Import/Paste Configuration dialog - Configure Programs tab:
  1. Select
    File > Import Component > <component>
    .
  2. Select a component for import and select
    Open
    .
  3. On the
    Import Content
    pane, select
    Programs
    .
Access imported programs through the
Programs
item in the
Import Content
pane. Selecting
Programs
shows a list of programs in a grid in the Details pane. When importing:
  • A single hierarchy - the programs grid shows the children of the program that is being imported into the project.
  • Multiple programs - the grid shows the programs that are being imported into the project.
  • Multiple hierarchies - the grid shows both the programs and the children of the programs that are being imported into the project.
Tag references are represented in the import content by the
Tags
item found under the
References
folder. Select
Tags
and the Details pane shows the tag references in the import content. The list includes any tags directly referenced by any imported logic and tags (through
Alias For
).
The
Tags
grid contains the union of all the program tags that are defined in both the import content and the project, and shows the disposition of each. Controller-scoped tag references that occur in the program's logic are represented on the tag references grid.
The
Operation
setting for these tags is based on the Operation chosen for the program that is being imported.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal