Import Configuration Dialog - Component References Overview

Use this dialog box to configure and view other components (references to tasks, programs, routines, or modules).
The Import Content shows the routine name (that the components are being imported into) and any references in the References folder (if there are any referenced tags, data types, Add-On Instructions, or other components).
When the routine is selected, the properties of the routine are displayed, along with information about how many components are being imported, and where they will be inserted.
Other Component are references via logic that does not exist in the import file and therefore only names are available. Other Component are components that are referenced by name in the imported logic, but whose definitions are not included in the import file. Configuring these components involves changing their final (if necessary) to cause them to associate with the right components in the project.
Examples of other Components are:
  • References to routines specified in instructions, such as JSR, FOR, SFR, SFP
  • References to a Task through an EVENT instruction
  • References to a phase though PCMD, PCLF, PATT, PDET, or POVR instructions
  • References to higher level components (for example, tasks, programs, or modules) through GSV and SSV instructions
Parameters
Row Header
The leftmost part of the grid, provides an indication of the condition of the component that was imported, as follows:
Import_Configuration_dialog_warning_flag_without_astericks
Indicates why the component needs attention. Hover the cursor over the red flag icon and a tool tip displays and indicates the reason for the message.
fixed_product_safety_warning
Indicates a safety warning.
Import Name
Displays the name of the component as read from the import file.
Operation
Displays either Use Existing or Undefined. See below for
Import Configuration Operations
for an explanation of these operations.
This field can only be changed by editing the contents of the Final Name field.
Final Name
The final name is the name as it appears in the project after the import. Changing the Final Name changes the name in all places where this component is referenced in the import content (throughout the logic and in any alias components).
You may modify the final name during configuration.
When you click in the Final Name cell, a pull-down menu appears. You can choose from the options in the pull-down menu, which provides a list of all the available components of this type in the project within the current scope (the type of browser varies with component type).
Class Name
Displays the class of the component that is referenced by the component reference in the import file.
Displays one of the following:
  • Task
  • Program / Phase
  • Module
  • Routine
Messages
Pay particular attention to warnings that appear in the area below the grid.
OK
Click this button to accept your import edits.
Cancel
Click this button to cancel your import and close this dialog box.
Help
Click this button for help on this dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal