Cannot Reschedule Existing Program or Equipment Phase (Online)

The program (or Equipment Phase) being imported already exists in the project, and is scheduled in a different location (task, unscheduled programs or phases, Controller Fault Handler, Power-Up Handler).
Programs and Equipment Phases cannot be rescheduled through import while online in run mode.
Proceed with the import, the Schedule In setting changes to the existing location and is unchangeable.
Use the option of changing the Final Name to create a new program or Equipment Phase, and then changing the Schedule In setting to the desired location.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal