Import/Paste Configuration dialog - Programs tab settings
This information describes imported program tags on the
Import Configuration - Programs
dialog box.Row Header
The leftmost part of the grid provides an indication of the condition of the component that was imported into the existing project, as follows:
![]() | Indicates why the component needs attention. Hover the cursor over the red flag icon and a tool tip appears and indicates the reason for the message. |
![]() | Indicates a safety warning. |
Import Name
Displays the name of the component as read from the import file.
An import name shows only for programs that exist in the project and in the import content.
Operation
Displays the operation for each tag. The operation is dependent upon the operation that is selected for the program being imported (that is, the
Operation
value on the Configure Program Properties
dialog box):- Create - for programs that exist in the import content but not in the project and the operation for the program is set toCreateorOverwrite.
- Discard - for programs that exist in the import content, but not in the project and the operation for the program is set toDiscardorUse Existing.
- Delete - for programs that exist in the project but not in the import content and the operation for the program is set toOverwrite.
- Use Existing - for each colliding program and the operation for the program is set toUse Existing.
- Overwrite - for each colliding program and the operation for the program is set toOverwrite.
Differences 

Indicates if there are differences between the program that is in the import content and the program that is in the project.
Also identifies if the program exists in the import content, or if it exists in the program that is in the project, or if it exists in both.
Click the browse button in the Details column to see details such as differences in connections, tags, or routines.
These icons provide an at-a-glance indication of how the imported content matches the content of the program that exists in the project:
![]() | Indicates a component that collides with another component, and has differences in the component definitions. |
![]() | Indicates a component that is present in the import content and not in the project. |
![]() | Indicates a component that is present in the project and not in the import content. |
Blank
(no icon) | Indicates a component that collides with another component, but has an identical component definition. |
Final Name
Shows the contents of the
Import Name
box, unless Operation
is set to Discard
or the program exists in the project but not in the import content (the Import Name
is blank).For cases where the program exists in the project but not in the import content, this box contains the name of the program in the project.
Details 

Select the browse button to open the
Collision
dialog box in which you view differences, if any, between the imported component and the existing component.- In theProperty Comparetab, a message is shown at the top of the dialog indicating whether there are differences in the property values between the imported component and the component that exists in the project. Where property values are different, the name of the property is shown in bold print and the row is highlighted.
- In theProject Referencetab, there is a cross reference listing of where the existing component is used in the project.
Inhibit
Shows if the program is selected as inhibited. An inhibited program does not execute until it is uninhibited.
If the
Operation
for the import is set to Create
or Overwrite
, you have the option to select or clear the check box to change the inhibit state of the program.The column is blank if the program is not inhibited.
Program Type
Shows the program type of the component from the import content if
Operation
is set to Create
, Overwrite
, or Discard
. Shows the program's type from the project if Operation
is set to Delete
or Use-Existing
.Parent Program
The program that exists in the import content becomes a child program of the parent program upon import.
If the program that exists in the import content is not imported into the program that is in the project, the program that is in the project is a child program of the parent program.
Scheduled In
Shows where the program that exists in the import content is scheduled upon import.
If the program exists in the project, and
Operation
is set to Use Existing
or Delete
, shows where the program that is in the project is scheduled. Description
Shows the description of the component.
Preserve existing tag values in offline project
Provide Feedback