Configure the Associated Axes and Control Mode

After you associate the axis to the drive, configure the axis and control mode.
To configure the Associated Axes and Control mode:
  1. From the
    Axis Properties
    dialog box, in
    Categories
    , click
    General
    .
  2. In the
    General
    area, from the
    Axis Configuration
    list, select the axis configuration type.
    TIP:
    The available
    Axis Configuration
    values are determined by the drive's profile and the default selection. If there is no drive associated with the axis, all values are available, and the default position is
    Position Loop
    .
  3. From the
    Feedback Configuration
    list, select the feedback configuration type.
    TIP:
    The
    Feedback Configuration
    values vary by profile and axis type.
  4. From the
    Application Type
    list, select the application type.
  5. From the
    Loop Response
    list, select the desired loop response.
  6. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal