Clear the fault and alarm log for an axis

Use the
Faults & Alarms
page in the
Axis Properties
dialog box to clear the faults and alarm logs in the controller for the axis. The last 25 faults and alarms display on the page, along with the time stamp, and the action taken in response to the event. Use the
Show
filters to toggle between displaying or hiding the fault and alarm conditions and the reset entries.
Before you begin:
  • The controller must be online. The page only shows entries when online with a controller.
Clear the fault and alarm log for an axis:
  1. In the
    Controller Organizer
    , expand the
    Motion Groups
    folder, and double-click an axis.
  2. From the
    Axis Properties
    dialog box, in
    Categories
    , click
    Faults & Alarms
    .
  3. Click
    Clear Log
    to clear the fault and alarm logs.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal