Routine Properties dialog box - General tab (Structured Text routine)

The General tab lists the properties associated with the selected structured text routine. The following table describes the dialog box parameters.
Parameter
Description
Name
The name of the routine.
Description
A description of the routine.
Type
Lists the type of routine (for example, ladder, function block diagram, sequential function chart, and structured text). For structured text, the verify state of the routine is displayed (Verified or Not Verified).
In Program
Lists the program to which the routine belongs.
Number of Lines
Displays the number of lines of text in the routine.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal