Use the Logical Organizer

The
Logical Organizer
is a graphical representation of the logical organization of your project called the logical model. It enables you to create and organize hierarchies of the programs and folders in your project, independent of the execution model.
Programs created in the
Logical Organizer
also appear in the
Controller Organizer
, but programs in the
Logical Organizer
that are used as folders do not appear in the
Controller Organizer
. You can do the following in the
Logical Organizer
:
  • Create a program, and use the program as a program or as a folder to organize other programs.
  • Add a routine to a program
  • Cut, copy, paste, and drag-and-drop programs, folders, and routines
  • Add and edit tags and parameters
  • Add and edit routine logic
  • Delete programs, routines
  • Navigate from a program or routine in the
    Logical Organizer
    to the same program or routine in the
    Controller Organizer
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal