Failed to set the Bit Number

You tried to set the value of the tag in the
Configuration
dialog box, but the operation did not succeed. This value represents a bit of a tag structure member. You might see this error when you select
Apply
, press Enter, or move off of one of the fields with a blue arrow. This could occur because:
  • The tag was deleted.
  • There is an invalid numeric value for the type of field (that is, if the field is expecting an integer and you enter a real value).
  • Insufficient memory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal