Update firmware revision

Use this procedure to update the firmware revision of the controller.
To update firmware revision:
  1. In the
    Who Active
    dialog box, select
    Update Firmware
    to open the
    Choose Firmware Revision dialog box
    .
  2. In
    Look for Firmware Update Files In
    , enter the directory where the firmware updates are stored.
    Select
    Browse
    to navigate to a specific directory.
  3. From the
    Revision/Update Type/File
    table, highlight the firmware revision to update the controller.
    Note that only those updates compatible with the version of software are listed in this table.
    TIP:
    Use Autoflash to update only the controller’s firmware. If there are other devices to perform firmware updates, run the ControlFLASH Plus application separately. Run the ControlFLASH Plus software by choosing
    Tools > ControlFLASH Plus
    .
  4. Select
    Update
    to start the flash upgrade.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal