Speed, acceleration, deceleration, and jerk enumerations

Speed enumerations
Common enumerations are used for the speed parameter of all motion instructions. Some instructions accept only limited subset of the speed enumerations. Checks for valid unit combinations are done at instruction execution time. Some enumerations that are in the following table are not used now but are reserved for future enhancements. Additional tables are given below that further clarify which combinations are accepted in MDSC mode and which are accepted in Time Driven Mode.
Enumeration
Definition
Mode
Compatibility
Note
0
1
2
3
Units per sec
% Maximum
Reserved
Reserved
Time Driven
Existing Enumeration
Existing Enumeration
New Enumeration
Reserved for Time based programming
4
5
6
7
Units per MasterUnit
Reserved
Reserved
Master Units
MDSC
New Enumeration
New Enumeration
Reserved for Time based programming
Follow these rules for Speed to determine allowable Time and MDSC Driven Mode:
  • When Speed is in either units/sec, %max, or seconds, then the instruction is considered to be in Time Driven Mode, regardless of the selection of units for acceleration, deceleration, or jerk.
  • When Speed is in either Master Units or in Units/MasterUnit, then the instruction is considered to be in Master Driven Mode, regardless of the selection of units for acceleration, deceleration, or jerk.
  • Speed, Acceleration, Deceleration, and Jerk must always be programmed in the same mode (Time Driven or Master Driven) or you get a runtime error.
  • When speed is specified in time unit seconds, the specified time is the total time of the move, including acceleration and deceleration time.
  • When speed is specified in Master distance units, the specified distance is the total master distance of the move, including acceleration and deceleration distance of the Master Axis.
Acceleration and deceleration enumerations
These enumerations are defined for Acceleration and Deceleration Unit parameters for motion instructions.
Enumeration
Description
Mode
Compatibility
Notes
0
1
2
3
Units per sec2
% Maximum
Reserved
Reserved
Time
Existing Enumeration
Existing Enumeration
Reserved for Time based programming
4
5
6
7
Units per MasterUnit2
Reserved
Reserved
Reserved
MDSC
New Enumeration
Reserved for Time based programming
This table shows acceptable combinations of Speed, Acceleration, and Deceleration units.
Acceleration and Deceleration Units
Units per sec
2
(Time Driven
Mode Units)
% Maximum
(Time Driven
Mode Units)
Seconds
(Time Driven
Mode Units)
Units per MasterUnit
2
(Master Driven
Mode Units)
Master Units
(Master Driven
Mode Units)
Speed Units
Units per sec
(Time Driven
Mode Units)
Existing Enumeration
Existing Enumeration
Not Implemented
Not allowed - Time and Master Driven Units may not be combined.
% Maximum
(Time Driven
Mode Units)
Existing Enumeration
Existing Enumeration
Not Implemented
Seconds
(Time Driven
Mode Units)
Not Implemented
Not Implemented
New Enumeration
Units per MasterUnits
(Master Driven
Mode Units)
Not allowed - Time and Master Driven Units may not be combined.
New Enumeration
Not Implemented
Master Units
(Master Driven
Mode Units)
Not Implemented
New Enumeration
These rules for Acceleration and Deceleration must be followed to determine allowable Time and Master Driven Mode:
  • Speed, Acceleration, Deceleration, and Jerk must always be programmed in the same mode or you get an error.
  • If Speed units are seconds, then acceleration, deceleration, and jerk units must be seconds too.
  • If Speed units are Master units, then acceleration, deceleration, and jerk units must be Master units too.
  • All unsupported unit combinations result in an error at runtime when the instruction is executed.
Jerk enumerations
The following enumerations are defined for time driven and MDSC driven Jerk units.
Enumeration
Description
Mode
Compatibility
Notes
0
1
2
3
Units per sec
3
% Maximum
% of Time
Reserved
Time
Existing Enumeration
Existing Enumeration
Existing Enumeration
Reserved for Time based programming
4
5
6
7
Units per MasterUnit
3
Reserved
% of Time-Master Driven
Reserved
MDSC
New Enumeration
New Enumeration
Reserved for Time based programming
Acceptable combinations of Accel and Decel Units are based on the programmed Speed Units in the instruction as is shown in the table below. Use this table to clarify the differences in the following four tables.
Speed Units
Accel Units vs Jerk Units Defined in Table:
Units per Sec
Table 1
Units per Master Units
Table 2
Seconds
Table 3
Master Units
Table 4
This table shows acceptable combinations of Acceleration Units and Jerk Units when Speed Units are Units per Sec.
Acceleration Units (Speed in Units per Second)
Units per sec
2
(Time Driven Mode Units)
% Maximum
(Time Driven Mode Units)
Seconds
(Time Driven Mode Units)
Units per MasterUnit
2
(Master Driven Mode Units)
Master Units
(Master Driven Mode Units)
This table shows acceptable combinations of Acceleration Units and Jerk Units when Speed Units are Units per Master Unit.
Acceleration (Speed in Units per Master Unit)
Units per sec
2
(Time Driven
Mode Units)
% Maximum
(Time Driven
Mode Units)
Seconds
(Time Driven Mode Units)
Units per MasterUnit
2
(Master Driven
Mode Units)
Master Units
(Master Driven
Mode Units)
Jerk Units
Units per sec
3
(Time Driven
Mode Units)
Incompatible combinations of Time and Master Driven Mode. An error occurs when you verify the routine.
Incompatible combinations of Time and Master Driven Mode. An error occurs when you verify the routine.
% Maximum
(Time Driven
Mode Units)
% of Time
(Time Driven
Mode Units)
Seconds
(Time Driven
Mode Units)
Units per MasterUnits
3
(Master Driven
Mode Units)
Incompatible combinations of Time and Master Driven Mode. An error occurs when you verify the routine.
New Enumeration.
Not Implemented
% of Time-Master Driven
(Master Driven
Mode Units)
New Enumeration.
Not Implemented
Master Units
(Master Driven
Mode Units)
Not Implemented
Not Implemented
The following table shows acceptable combinations of Acceleration Units and Jerk Units when Speed Units are in Seconds.
Acceleration (Speed in Seconds)
Units per sec
2
(Time Driven
Mode Units)
% Maximum
(Time Driven
Mode Units)
Seconds
(Time Driven Mode Units)
Units per MasterUnit2
(Master Driven
Mode Units)
Master Units
(Master Driven
Mode Units)
This table shows acceptable combinations of Acceleration Units and Jerk Units when Speed is in Master Units.
Acceleration (Speed in MasterUnits)
Units per sec
2
(Time Driven
Mode Units)
% Maximum
(Time Driven
Mode Units)
Seconds
(Time Driven Mode Units)
Units per MasterUnit
2
(Master Driven
Mode Units)
Master Units
(Master Driven
Mode Units)
Jerk Units
Units per sec
3
(Time Driven
Mode Units)
Incompatible combinations of Time and Master Driven Mode. An error occurs when you verify the routine.
Incompatible combinations of Time and Master Driven Mode. An error occurs when you verify the routine.
% Maximum
(Time Driven
Mode Units)
% of Time
(Time Driven
Mode Units)
Seconds
(Time Driven
Mode Units)
Units per MasterUnits
3
(Master Driven
Mode Units)
Incompatible combinations of Time and Master Driven Mode. An error occurs when you verify the routine.
Not Implemented
Not Implemented
% of Time-Master Driven
(Master Driven
Mode Units)
Not Implemented
New Enumeration.
Master Units
(Master Driven
Mode Units)
Not Implemented
New Enumeration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal