Create a folder
    Create a folder to contain nodes in your project.
You can create multiple versions of any folder. When you create a folder, the folder automatically has a context menu that you can right-click to create items specific to that folder category. Each folder category  has an icon before it.
- InProject view, create either:- Folder. Right-click the node to contain the folder and then select .
- Category folder. Right-click the project level node, selectNew, and then select the category of folder.
 
The 
NewFolder#
 appears in Project view
.folder
    
Provide Feedback