Configure a PDF viewer
    Add a PDF viewer to insert an empty container for a PDF file and then specify the PDF file to display. You can display PDF files local to the project or remote PDF files.
- InProject view, inUI, right-click a container and then select .
- InProperties, setZoom mode:- Fit width. PDF document fits the page width.
- Fit height. PDF document fits the page height.
- Fit page. PDF document fits the page width and height.
- Actual size. Actual size of the PDF document displays in the PDF viewer container.
- Custom level. Specified zoom level of the PDF document displays in the PDF viewer container.
 
- InPath, either:- SelectBrowseand select the local PDF file to display.TIP:To find items, start typing the item name to find inSelect file.If the file does not appear inSelect file, selectand in Import file(s)Import file(s), select the file to import and then chooseSelect. Import file(s)Import file(s), select the file to import and then chooseSelect.
- Enter the address of the remote PDF file to display.TIP:PDF viewer supports these protocols for displaying remote PDF files:- http
- https
 
 
- (optional) To display the PDF document on a specific page, setCurrent Pageto the page to display.For example, to display the PDF document on page 5, enter5.
- (optional) Set theAppearanceandSize and layoutproperties.
pdf
    
Provide Feedback