Move an object
    Move an object in the editor to position objects as they will appear at runtime. All of the objects in a container move with the container.
- To move an object
- In the editor, select and drag the object.
- InProject view, select the object and then inPropertieschange:- Horizontal alignment. Enter the value for the space between the object and the X-axis.
- Vertical alignment.Enter the value for the space between the object and the Y-axis.
 TIP: The position of the object inProject viewdetermines the order of objects on the Z-axis compared to other objects in the same container. Objects lower in the tree appear higher in the order on the Z-axis.
move
alignment
    
Provide Feedback