The attempted command cannot be executed as the axis type is not servo

Certain commands, such as Tune, are not available if the axis type is not servo. Either change the axis type to servo, or select a different command.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal