Make Viewable command
Select
Make Viewable
to enable users to view the logic and local tags on a system without the source key required to access the component.
TIP:
Make a component viewable by selecting
Allow viewing of component(s)
when applying a source key to the component.
IMPORTANT:
Make Viewable
does not apply to license protected components. To view a license protected component, insert a CmStick
containing the license with at least View permission into any USB port on the computer.Provide Feedback