Invalid Find Where value
The Find Where field must match the context and type of the selected item in the Organizer (either the Controller Organizer or the Logical Organizer). For example, if the Find Where field is set to All Programs in Current Program, a program or one of its child
routines must be selected in the Organizer.
program
A program executes a set of instructions in a project.
routine
A sequence of logic that is executed as a block.
Provide Feedback