Forced Use Existing

When performing an import in Run mode, pay particular attention to the configuration of the import.
  • Programs cannot overwrite Equipment Phases and vice versa.
  • Routines cannot overwrite routines of a different type (that is, a Ladder Diagram cannot overwrite a Function Block Diagram).
  • Do not overwrite a program if the assigned routines are different. The existing program is used.
  • Do not overwrite a tag online that already exists in the project and has a different data type. The existing program is used.
If collisions occur, the operation for the component is forced to
Use Existing
. It is important to review how the other components are configured. It is also important to understand the impact of importing the other components without importing the discarded component.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal