Equipment Sequence Monitor

Open the
Equipment Sequence
Monitor
by opening an
Equipment Sequence
diagram from the
Controller Organizer
or
Logical Organizer
, and going on line with the controller. The
Equipment Sequence
Monitor
is the routine window.
The
Equipment Sequence
Monitor is the online version of the
Equipment Sequence
Editor and is used to monitor and interact with Equipment Sequences that have been downloaded to the controller. The control engineer can do the following:
  • Command the Equipment Sequence.
  • Change the value of parameters and attributes.
  • Interact with the executing sequence.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal