Create a button that shuts down the host system
Add a button that shuts down the host operating system on which the
FactoryTalk Optix Application
runs.
IMPORTANT:
Pressing
Shut down system
immediately shuts down the host operating system
on which the FactoryTalk Optix Application
runs.- InProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the button, select, and enter
ShutDownSystemButton. - InProperties, setTexttoSHUT DOWN HOST SYSTEM.
- InEvents, next toMouseClick event, selectand select .

Provide Feedback