Create a button that closes the application
Create a button that closes the
FactoryTalk Optix Application
application.- InProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the button, select, and enter
CloseApplicationButton. - InProperties, setTexttoClose application.
- InEvents, next toMouseClick event, selectand select .

Provide Feedback