Add users
Add users with different locales.
Prerequisites
Add the it-IT locale. See Add a locale language to a localization dictionary.
- To add users
- InProject view, expand theSecurityfolder.
- Create two users by right-clickingUsersand selecting .
- Rename the users by hovering-over each user, selecting, and entering:

- Alice
- Tim
- InProject view, selectAlice.
- InProperties, setLocaletoit-IT.
Provide Feedback