Create Motor objects
Create motor objects to populate panel instances with sample data.
- Create a Motor type:
- InProject view, right-clickModeland select .
- Hover-over the object, select, and enter
Motor. - InProperties, at the top, a variable by selectingand selecting
Variable. - Rename the variable by hovering-over the variable, selecting, and entering
Speed - InType view, double-clickModel.
- FromProject view, dragMotorto theTypesfolder inType view.
InProject view,Motor (type)andMotorInstanceappear. - Create Motor instances:
- InProject view, hover-overMotorInstance, select, and enter
Motor1 - Right-clickModeland select .InProject view,Motor2appears.
- For each Motor instance, inProperties, set anySpeedvalues.
- Create a Motor_Ext type:
- InProject view, right-clickModeland select .
- Hover-over the object, select, and enter
Motor_Ext - InProperties, at the top, add two variables by selectingand selecting
Variable. - Rename the variables by hovering-over each variable, selecting, and entering:

- Acceleration
- Power
- FromProject view, dragMotor_Extto theTypesfolder inType view.
InProject view,Motor_Ext (type)andMotor_ExtInstanceappear. - Create Motor_Ext instances:
- InProject view, hover-overMotor_ExtInstance, selectand enter
Motor1_Ext - Right-clickModeland select .
- InProject view, hover-overMotor_Ext1, selectand enter
Motor2_Ext - For each Motor_Ext instance, inProperties, set anyAccelerationandPowervalues.
Provide Feedback