Create an acceleration gauge and labels
- Create the speed gauge:
- InProject view, right-clickMotorAccelerationPaneland select .
- Hover-over the gauge, select, and enter
AccelerationGauge. - InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
- Create the speed label:
- InProject view, right-clickMotorAccelerationPaneland select .
- Hover-over the label, select, and enter
AccelerationLabel. - InProperties, setTexttoAcceleration.
- Create the speed value label:
- InProject view, right-clickMotorAccelerationPaneland select .
- Hover-over the label, select, and enter
AccelerationValueLabel. - InProperties, create a dynamic link betweenTextand .For more information about dynamic links, see Create dynamic links.
Provide Feedback