View committed changes
View the committed changes of the open project by viewing the project history.
- In the toolbar, select.
View history - InVersion history, select a commit.TIP:represents a change that is committed to the local repository and
Local historyrepresents a change that is pushed to the remote repository.
Remote historyThe changes in the commit appear highlighted. - Expand a highlighted object to view the changes in the object.TIP: Values that change in an object are crossed out and an arrow points to the new value.
Provide Feedback