Pull changes
Pull changes to view updates and conflicts between the remote and local repositories.
Use Pull preview to accept updates and resolve conflicts.
TIP:
When there are changes to pull from the remote
repository, the message
indicates that there is one commit that is ready to pull.
Remote changes available to pull
appears
in the status bar and the Pull from remote
icon displays a blue number
with the number of commits to pull. For example, Pull from remote
Prerequisites
- Configure your user identities for version control providers. See Configure version control.
- If prompted, commit local changes before pulling remote changes.
- To pull changes
- In the open project, select.Pull from remoteChanges and conflicts between the local project and the project in the remote repository appear highlighted inPull preview. For more information, see Pull preview.TIP: A conflict may occur if a property value in both the remote project and the local project has changed. A conflict may also occur if an object is removed in one version of the project and the same object is modified in the remote repository. Highlighted conflicts display changed values and removed objects that are crossed out. The number of conflicts appears in the status bar.
- (optional) At the top ofPull preview, select the content to view:
- All. All project content in both the local and remote projects.
- Updates. Only changes in the local and remote projects.
- Conflicts. Only conflicts between the local and remote projects.
- Expand a highlighted conflict to display the values in conflict.
- (optional) At the top of the preview, selectto navigate and expand the next conflict orto navigate to the previous conflict.TIP: An icon in a row inPull previewindicates:
- A conflict exists between the local and remote repository.
- A conflict was resolved by selecting either the local or remote change in the row.
- A change exists in the local or remote repository.
- An object was added.
- An object was removed.
- In each highlighted row, select the version of content to keep:
- Individual local change. In a highlighted row, select the local changeon the left.
Local history - Individual remote change. In a highlighted row, select the remote changeon the right.
Remote history - All local changes. At the top of the preview, selectTake all local.
- All remote changes. At the top of the preview, selectTake all remote.
- SelectAcceptto accept the selected changes, or selectCancelto reject all of the conflicts in the remote project and retain the values in the local project.
The project opens and the message
The project is
synchronized
appears in the status bar.update
pull
Provide Feedback