Create an object
Create an object to add a node to the project.
- InProject view, select the folder in which to create the object, and then selectin the
Project viewtoolbar.TIP: You can also right-click a folder inProject viewand use theNewcontext menu to create objects.The context menu displays objects that the folder can contain based on the folder category. - Select the object to add to the project.
- (optional) InProperties, select, select
Display name, and enter the display name. - (optional) InProperties, select, select
Description, and enter the description.
The new object appears in
Project view
. The hover-over tooltip shows the display name and description.
object
Provide Feedback