Search for nodes
Use
Search
in Project view
to search for and filter project nodes in the tree structure.- InProject view, perform any of the following:
- To search for project nodes, inSearch, enter a search query.
- To clear the search query, inSearch, select.

- To filter project nodes by type, inSearch, selectand then select or clear the node types to include in the query.

- To clear all filters, inSearch, selectand then select
Clear All Filters.
You can search for project nodes using theirNodeID, by enteringn:Node_IDFor example:n: 85/00000000000123456TIP: You can also enter just the numeric string after the "/" as your search query. The string is unique for each project node.For example:n: 00000000000123456At least 4 characters of the NodeID are required to trigger the search. You can also search bynamespaceonly, for examplen: 8/orn: 123/, with no length requirement, but this search may take more time.
search
Provide Feedback