Certificate errors
Certificate errors may display when using the web browser object.
Certificate errors that are ignored at runtime when
Ignore invalid CA
errors
is set to True
. For more information, see Configure a web browser.Error | Description |
|---|---|
CertificateAuthorityInvalid | Certificate not signed by a trusted CA |
Certificate errors listed in
Certificate error
. To ignore the
errors, select Accept the risk and continue
at runtime.Error | Description |
|---|---|
SslPinnedKeyNotInCertificateChain | Certificate does not match the built-in public keys pinned for the host name |
CertificateCommonNameInvalid | Certificate common name does not match host name |
CertificateDateInvalid | Certificate is not valid at the current date and time |
CertificateAuthorityInvalid | Certificate not signed by a trusted CA |
CertificateContainsErrors | Certificate contains errors |
CertificateNoRevocationMechanism | Unable to determine if the certificate is revoked |
CertificateUnableToCheckRevocation | Unable to get revocation information for the certificate |
CertificateRevoked | Revoked certificate |
CertificateInvalid | Invalid certificate |
CertificateWeakSignatureAlgorithm | Certificate signed with a weak signature algorithm |
CertificateNonUniqueName | Certificate host name is not unique |
CertificateWeakKey | Certificate contains a weak key |
CertificateNameConstraintViolation | Certificate claimed DNS names violate name constraints |
CertificateValidityTooLong | Too long certificate validity period |
CertificateTransparencyRequired | Unable to get required certificate transparency information from the server |
CertificateKnownInterceptionBlocked | Certificate known for interception by an entity other than the device owner |
certificate
Provide Feedback