Configure the editor grid
Configure the grid in the editor to show or hide the grid, align objects in the grid, and size the grid.
- InProject view, double-click a container object, or select.
The editor opens in a new tab. - In the editor toolbar, select.
Grid settings - Select the option to configure the grid:
- Grid Visible. Toggle showing the grid in the editor.
- Snap to grid. Align the edges of objects with the grid.
- Grid size. Specify the size of the grid in pixels.
grid
editor grid
Provide Feedback