Dynamic links
Dynamic links join a parent node (variable) with a source node (another variable or object property).
TIP:
Generally, use a dynamic link to set a variable value based on:
- The value of another variable.
- A property of an object.
For example, set the text property of a label object based on the value of a temperature variable.
Source types and values
By default, depending on the dynamic link source node type, its source value is set as follows:
Dynamic link source node type | Dynamic link source value |
|---|---|
Variable | The Value attribute of the variable. |
Object | The NodeId property of the object. |
Modes
The mode of a dynamic link specifies its direction:
- Read

- Read from the source node to the parent.Default for dynamic links defined in NetLogics.
- Write

- Write from the parent to the source node.
- Read/write

- Read from the source node to the parent and write from the parent to the source node.Default for dynamic links created inFactoryTalk Optix StudioUI.
Complex dynamic links
A complex dynamic link involves transformations of the source node value through converters. See Converters.
You create complex dynamic links by using the Complex Dynamic Link Editor. See Complex dynamic link editor.
NOTE:
If you set a dynamic link between a graphical object property and another node, the parent node is always the graphical object property. If the parent or source node of a dynamic link is an array variable, you can set a specific array cell as the parent or source value.
Provide Feedback