Create a dynamic link using an alias
Create a dynamic link to use an existing alias as a shortcut. Dynamic links help prevent having to look up the same source node repeatedly.
- InProject view, select a node that has the property value that you want to set through the dynamic link.
- InProperties, in the property of interest, select.
Add Dynamic Link - Expand either theAliasesfolder or thePanel loadersfolder to select the alias nodeto display.
The information model to which the alias points and the source node of the dynamic link appear.TIP: In thedynamic linkswindow, the aliases that you create appear in theAliasfolder. Aliases in theDynamic panelfolder are generated automatically. - Select the source node of interest and then chooseSelect.
The path to the reference node or attribute appears in the property.
dynamic link
Provide Feedback