Fiber-optic Transceiver Circuit Board Status Indicators
PowerFlex®
755T fiber-optic transceiver circuit boards use status indicators to report conditions. The fiber-optic transceiver circuit boards plug into edge connectors on the fiber interface circuit board in the control pod assembly of frame 7…15 drives and bus supplies.Fiber-optic Transceiver Status Indicators
Color | State | Description |
|---|---|---|
Green | Flashing | Fiber connection is online. |
Red | Flashing | Fiber connection is offline. |
Provide Feedback