Safety Applications
The safety concept assumes the following requirements:
- You are responsible to create, operate, and maintain the safety application.
- You are fully qualified, specially trained, and experienced in safety systems.
- You apply the logic correctly to detect programming errors through strict adherence to specifications, programming, and naming rules.
- You perform a critical analysis of the application and use all possible measures to detect a failure.
- You confirm all application downloads via a manual check of the safety signature.
- You perform a complete functional test of the entire system before the operational startup of a safety-related system. This test includes, but is not limited to, the following:
- Validate that the overall functionality of the implemented safety functions, including I/O configuration via Add-On Profiles, beyond the limits of the individual devices (boundary testing).
- Verify that the correct versions of software are used.
Controller Mode | Controller Safety Execution |
|---|---|
Program |
|
Test |
|
Run |
|
Unlocked no signature | Only for development purposes |
|
Locked no signature | Only for development purposes |
|
Unlocked with signature | SIL 2/SIL 3 (per controller) |
|
Locked with signature | SIL 2/SIL 3 (per controller) |
IMPORTANT:
If the controller is safety-locked and the safety-unlock password is lost and a download is needed, you must perform a Stage 1 reset of the controller.
|
Provide Feedback