Failed to modify operand

Tried to modify the value of an operand or tag, but the operation failed. This could occur because:
  • the operand does not contain a valid tag
  • the tag is a structure of some type
  • the value is not a valid value for the type of tag (for example, the value may not be a valid integer value for a SINT tag)
  • the tag was deleted (for a program scoped tag)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal