Motion Arm Watch (MAW)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580, and
GuardLogix
5580 controllers. Controller differences are noted where applicable.
Use the Motion Arm Watch (MAW) instruction to arm motion module watch position event checking for the specified axis. When this instruction is called, a watch position event is enabled using the watch Position for the Axis and specified Forward or Reverse event condition. After the arming is complete the Actual Position for the Axis is monitored against the Watch Position and when the specified watch event condition is met, the Event (PC) bit is set, and the Watch Event Status bit in the Axis data structure is set.
Architecture and safety support
Architecture
Standard
Safety
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Yes
No
Compact GuardLogix 5380, CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers
Yes
No
Available Languages
Ladder Diagram
MAW_LD_avail_v31
Function Block
This instruction is not available in function block.
Structured Text
MAW(Axis,MotionControl, TriggerCondition,Position);
Operands
Ladder Diagram and Structured Text
Operand
Type
CompactLogix
5370,
Compact GuardLogix
5370,
Compact GuardLogix
5380,
CompactLogix
5380,
CompactLogix
5480
Type
ControlLogix
5570,
GuardLogix
5570,
ControlLogix
5580, and
GuardLogix
5580 controllers
Format
Description
Axis
AXIS_CIP_DRIVE
AXIS_CIP_DRIVE
AXIS_SERVO
AXIS_SERVO_DRIVE
AXIS_GENERIC_DRIVE
AXIS_GENERIC
Tip:
AXIS_GENERIC is supported by the
ControlLogix
5570 and the
GuardLogix
5570 controllers only.
Tag
Name of the axis on which to perform operation. For controllers that support the REF_TO motion data types, the supported axis operand type can be replaced by an equivalent REF_TO type.
Motion Control
MOTION_INSTRUCTION
MOTION_INSTRUCTION
Tag
Structure used to access instruction status parameters.
Trigger Condition
BOOLEAN
BOOLEAN
Immediate
Select the watch-event trigger condition:
0 = forward – the servo module looks for the actual position to change from less than the watch position to greater than the watch position.
1 = reverse – the servo module looks for the actual position to change from greater than the watch position to less than the watch position.
Position
REAL
REAL
Immediate or Tag
The new value for the watch position.
See
Structured Text Syntax
for more information on the syntax of expressions within structured text.
For the operands that require you to select from available options, enter your selection as:
This Operand
Has These Options Which You
Enter as Text
Or Enter as a Number
TriggerCondition
forward
reverse
0
1
MOTION_INSTRUCTION Structure
Mnemonic
Description
.EN (Enable) Bit 31
It is set to true when the rung makes a false-to-true transition and remains set to true until the servo message transaction is completed and the rung goes false.
.DN (Done) Bit 29
It is set to true when the axis watch event checking has been successfully armed.
.ER (Error) Bit 28
It is set to true to indicate that the instruction detected an error, such as if you specified an unconfigured axis.
.IP (In Process) Bit 26
It is set to true on positive rung transition and cleared to false after the watch event has occurred, or has been superseded by another Motion Arm Watch, or terminated by a Motion Disarm Watch command.
.PC (Process Complete) Bit 27
It is set to true when a watch event occurs.
Description
The MAW instruction sets up a Watch Position event to occur when the specified physical axis reaches the specified Set-point position.
Set Point Position
Watch Position events are useful for synchronizing an operation to a specified axis position while the axis is moving, such as activating a solenoid to push a carton off a conveyor at a certain axis position. Select or enter the desired physical axis, the desired Trigger Condition, and enter a value or tag variable for the desired Watch Position.
If the targeted axis does not appear in the list of available axes, the axis has not been configured for operation. Use the Tag Editor to create and configure a new axis.
When an Arm Watch Position instruction is executed, the WatchEventStatus bit is set to 0 (FALSE) and the actual position of a physical axis is monitored (at the servo loop update rate) until it reaches the specified Watch Position. After the watch position event occurs, the WatchEventStatus bit for the axis is set to 1 (TRUE).
Multiple watch position events may be active at a given time, however only one may be active at a time for any given physical axis. Each event is monitored independently and may be checked using the appropriate WatchEventStatus bit.
IMPORTANT:
In large I/O connections, force values can slow down the rate at which the controller processes repetitive watch positions.
To successfully execute a MAW instruction, the targeted axis must be configured as either a Servo or Feedback Only axis. Otherwise, the instruction errs.
IMPORTANT:
The instruction execution may take multiple scans to execute because it requires multiple coarse updates to complete the request. The Done (.DN) bit is not set immediately, but only after the request is completed.
In this transitional instruction, the relay ladder, toggle the Rung-condition-in from cleared to set each time the instruction should execute.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized reference or a reference of incorrect type is passed to the Axis Operand. See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
The .EN, .DN, .ER, and .IP bits are cleared to false.
Rung-condition-in is false
The .EN bit is cleared to false if the .DN or .ER bit is set to true. Otherwise, the .EN bit is not affected.
The .DN,.ER ,.IP and .PC bits are not affected.
Rung-condition-in is true
The .EN bit is set to true and the instruction executes.
Postscan
N/A
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Ladder Diagram table.
Normal execution
See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table.
Postscan
See Postscan in the Ladder Diagram table.
Error Codes
See Motion Error Codes (ERR) for Motion Instructions.
Extended Error Codes
Extended Error Codes provide additional instruction specific information for the Error Codes that are generic to many instructions. The following Extended Error codes help to pinpoint the problem when the MAW instruction receives a Servo Message Failure (12) error message. See
Motion Error Codes (.ERR)
for Motion Instructions.
Associated Error Code (decimal)
Extended Error Code (decimal)
Meaning
SERVO_MESSAGE_FAILURE (12)
No Response (2)
Not enough memory resources to complete request. (SERCOS)
Status Bits
MAW Changes to Status Bits
Bit Name
State
Meaning
WatchEventArmedStatus
TRUE
The axis is looking for a watch position event.
WatchEventStatus
FALSE
The previous watch event is cleared.
Example
Ladder Diagram
MAW_LD_ex_v31
Structured Text
MAW(Axis1,MAW_1,Forward,fwdmvpos_1);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal