Edit the logic for the definition of an Add-On Instruction
Open the logic for the definition of an Add-On Instruction to edit the local tags and logic of the Add-On Instruction. Changes made to the definition of an Add-On Instruction appear in every instance of the Add-On Instruction in the project.
- Open the logic for either:
- Definition of an Add-On Instruction. On the explorerbar, select
Library, expand the Add-On Instruction, and then selectLogic. - Instance of an Add-On Instruction:
- On the explorer bar, select
System. - InSystem, expand theFactoryTalk Smart Objectand then program and then double-click the routine.
- In the upper-right corner of the tab for the routine, select the drop-down and then select the definition of the Add-On Instruction at the top of the list.
- Edit the logic for the Add-On Instruction.TIP: An Add-On Instruction cannot contain logic that directly or indirectly references itself.
Provide Feedback