Delete the definition of an Add-On Instruction
Delete an Add-On Instruction to remove it from the project. Deleting an Add-On Instruction removes all instances from the project. Remove an Add-On Instruction from
Library
in the current project. You cannot delete the definition of an Add-On Instruction from a project that contains instances of the Add-On Instruction. To delete the definition of an Add-On Instruction, remove all instances of the Add-On Instruction from the project.
To delete the definition of an Add-On Instruction
- On the explorerbar, select
Library. - InLibrary,expandAdd-On Instruction.
- Right-click the Add-On Instruction to delete and selectDelete. The messageDelete all instances of the add-on instruction from the projectappears.
- SelectDeleteto delete the Add-On Instruction from the project, orCancelto leave the Add-On Instruction in the project.
Provide Feedback