Factors That Affect Logix Reaction-time Components
A number of factors can influence the Logix system reaction time components.
Network traffic and EMC create a lower limit for the values that you can successfully use for the timeout multiplier and network delay multiplier.
Reaction Time Component | Factors |
|---|---|
Safety task reaction time | Safety function muting during qualification, loss of redundancy, or a lock for update impacts the safety task reaction time in high demand applications. |
Input device delay |
|
Safety input connection reaction time limit |
|
Safety task period and safety task watchdog |
|
Output connection reaction time limit |
|
Output module delay | Output module reaction time |
Provide Feedback