Safety Application Suitability Levels
Suitability Level | Conditions | Notes |
|---|---|---|
Applications that are rated up to, and including, SIL 2 as
defined in IEC 61508, and PLc, Cat. 2 as defined in ISO
13849-1 | The modules uses single-channel mode:
| Consider the following:
The larger safety system within which the safety I/O module
resides can provide the diagnostics necessary to achieve the
stated Suitability Level without the requirement that Point mode
be Safety Pulse Test. To achieve the specific Safety Integrity Level, see the wiring
diagrams for the respective safety module. |
Applications that are rated up to, and including, SIL 3 as
defined in IEC 61508, and PLe, Cat. 4 as defined in ISO
13849-1 | The modules use single-channel mode:
The modules use dual-channel mode:
The modules use dual-channel mode:
|
Provide Feedback